Showing results for 
Search instead for 
Do you mean 
Reply
Solved! Go to solution

New message on assembly expression

Hi,

there is an option to avoid showing the message attached in the picture ?

 

Thank you...

Using NX 10 / RuleDesigner PDM

Testing NX 11 on production
Testing NX 12 Beta on production
18 REPLIES

Re: New message on assembly expression

Hi cubalibre00,

I'm not sure if there is a way and this is really annoying. At least it should not prevent assemblies to fully open.

Laurenj

Re: New message on assembly expression

Hi @cubalibre00 and @laurenj,

 

Please have a look at this FAQ in our Solution Center:

http://solutions.industrysoftware.automation.siemens.com/view.php?si=001-7609311

 

I think it will solve your problem.

 

Kind regads,


Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: New message on assembly expression

Thanks for the link Dennis,

I don't really mind the dialog, but what annoys me is the fact, that it prevents the assy to fully open. You have to click on the OK button for that. It should be like a non-modal info/warning dialog. I'm planning to submit an ER for that.

Re: New message on assembly expression

Hello @laurenj,

 

If you look at the last line of the FAQ. It says there is an enhancement on it's way in one of the newer releases of NX 10. i believe a Customer default. But i would need to check for the details.

 

Kind regards,


Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: New message on assembly expression

Oh sorry! I stop reading at "... customer default option" and skipped the end to check the env variable. No surprised I was asking myself where was the customer default option!

Re: New message on assembly expression

Just checked, And yes there will be a Customer default in NX 11.0

Customer Defaults -->  Gateway --> General --> Expressions --> Show Missing Interpart Expression Part Warnings.

 

Looking at your remark again. But the variable and the Customer Default, will both prevent the warning completly. And I believe you do want the warning, but in the background want NX to continue loading the assembly.

 

This you should request via an ER indeed.

 

Kind regards,

 

Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: New message on assembly expression

Hi Dennis,

this variable is set on our shared UGII_ENV_FILE, but doesn't work.

Must be set on the environment variable of the computer ?

The NX version is the last 10.0.3.5 SP 3

Thank you...

Using NX 10 / RuleDesigner PDM

Testing NX 11 on production
Testing NX 12 Beta on production

Re: New message on assembly expression

[ Edited ]

Hi @cubalibre00,

 

Normally I would say, it should not matter. First I would check if you have the correct variable, and value:

UGII_KF_DISABLE_MISSING_IPE_PART_WARNINGS=1

If so and it does not work from the UGII_ENV_FILE, please try it as system variable.

The version you are using, should work as far as I know. Or else check for the Customer default, might have just been introduced in the MP as well.

 

Kind regards,

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: New message on assembly expression

Should have checked this first, but the Customer Default is not in NX 10.0.3 MP3. Just in NX 11.0.

So please check the variable, and if a system variable does work. I have no assembly to check the problem.
Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software