Cancel
Showing results for 
Search instead for 
Did you mean: 

New physical measure -> Surface power density

Valued Contributor
Valued Contributor

Hello,

I am looking for a solution to define a variable whose physical dimension is a "Surface power density" .

That is "W/m^2"  or  also  "kg/m^3".

I don't find this measure in the list then I write an expression.

Thank you for your help.

3 REPLIES 3

Re: New physical measure -> Surface power density

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi serrep,

 

In the Dimensional Column from the dropdown first define Heat Flux resp. Mass Density then define your units in the Unit column.

 

Best Regards

Fred

 

2019_01_21_17_53_10_NX_12_Modeling.png

Re: New physical measure -> Surface power density

Valued Contributor
Valued Contributor

Thank you,

The dimensionality "Heat Flux" is correct.

I have made a mystake with the other physical dimension. It was "kg/s^3" and not "kg/m^3".

Best Regards

Philip

Re: New physical measure -> Surface power density

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @serrep,

 

I had same difficulty to find out from >50 dimensionality types (being new to expressions). So to find out correct type:

  • exported existing expressions to .exp file
  • according to syntax put new expressions values like below:
[W/m^2]test1=202
[kg/m^3]test2=202
[kg/s]test3=202
  • Imported the .exp file again & NX has created expressions using matching types like shown in image below.

Shared above scenario, this will certainly be helpful to someone ahead.

 

NX gives error while importing expression with unit "kg/s^3", this indicates there doesn't exists dimensionality for this.

 

Regards,
Samadhan

Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

 

Expressions.JPG

 

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!