Cancel
Showing results for 
Search instead for 
Did you mean: 

Non printable note in NX drafting?

Creator
Creator

Hi,

 

any idea if we can set a note/annotation in NX drafting to be non printable? so that when the user print out the drawing the particular note does not get printed out?

 

i am currently using NX8.5.3.3

 

thank you!

6 REPLIES

Re: Non printable note in NX drafting?

Siemens Phenom Siemens Phenom
Siemens Phenom

You could add those notes a specific layer and then use a Journal to print the Drawing that would make that particular layer invisible before generating the print file, then set it visible again afterwards.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: Non printable note in NX drafting?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Should be a nice enhancement that you can set which layers you don't won't to export/Print like in the step export.


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Non printable note in NX drafting?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Until, of course, a crucial note gets put on the wrong layer, and the vendor making the part for you makes 1000s of parts to the "without note" condition, because that's the drawing they got. 

 

Just curious - why would you NOT want to print a note that is on the drawing?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Non printable note in NX drafting?

Creator
Creator

Hi John,

 

Thank you for your input.

 

Jasons

Re: Non printable note in NX drafting?

Creator
Creator

Hi Ken,

 

Most of the time it is for the engineers to "pass" down some messges/notes to take note some of the issues that the current drawing or designs may have, or some of the infomation on the drawing might not be meaningful to the customers when we print out.

 

Jasons

Re: Non printable note in NX drafting?

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

I do this all the time and place my notes outside of the print border. We have even had a set of check boxes in the upper RH corner of the drawing where the boxes were on the printable sheet while the text for each of the boxes was outside the printable area. 

 

Notes on the side.jpg