Cancel
Showing results for 
Search instead for 
Did you mean: 

Not a part file?

Experimenter
Experimenter

Hi I am trying to load an assembly. I have all the part files under the same folder, using the load from folder option, but there are four parts that do not load and the only error is that they are "Not a part file" even though they are named as a .prt file and recognized as a UG part file.

 

Does anyone know the reasons for this? I have had this happen before and I simply clicked the generate missing part members in the load options menu and it solved the issue. This time it is not helping.

2 REPLIES

Re: Not a part file?

Siemens Phenom Siemens Phenom
Siemens Phenom

What happens if you try to open the 4 files individually?

 

 

Re: Not a part file?

Experimenter
Experimenter

The same error happens when I tried to do that. I had this happen with previous files but it was corrected when I chose an option in the load options.

 

I used the Utils that come with NX to check the part files, they are corrupted. Turns out the way that my co-worker and I were transferring files was corrupting the files. We used a more direct way and now the files are fine.