Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Not tangent Fillet

Creator
Creator

Hi,


I'm in need of a Fillet that is tangent on one side and it is not tangent on the other side, like in the attached screenshot.

 Fillet.pngFillet

I want to obtain this fillet but if possible with the Fillet command on a 3D part not with a sketch and extrude.

Thanks.

6 REPLIES 6

Re: Not tangent Fillet

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

Can you provide us with some of your use cases also?

In the mean time you can use this as a workaround.

force_roll.jpg

 

Thanks and Best Regards

Kapil

Re: Not tangent Fillet

Creator
Creator

Hi Kapil,

 

Fillet_bp.png

 

This is the concrete example where I need said fillet, also the revolved parts interior is built as the previously attached sketch.


In the meantime I will try your solution hope it works.

Also I have NX set to german and unfortunately can't change it to english.

Thanks! 

Re: Not tangent Fillet

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Ddzed
ok...do let us know if you have some issues.

Best Regards

Kapil

Re: Not tangent Fillet

Creator
Creator

So, your option sadly doesn't work, or at least I'm not able to do it. Also I'm using NX9, does that have to do something with it? while the option for the Blend Continuity, G1 Tangent, does not appear for me. 

Only these two options appear:

Fillet_options.png

Re: Not tangent Fillet

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi 

 

Re: Not tangent Fillet

Creator
Creator

Thats it! It's exactly what I wanted, maybe not the most aesthetically pleasing solution but it work just fine.
Thanks a lot! Smiley Happy