Cancel
Showing results for 
Search instead for 
Did you mean: 

Note - Insert text from file

Valued Contributor
Valued Contributor

Anyone else noticed that the Insert text from file function does not work in NX9.03 with Teamcenter10 in the Note command?

 

Has been reported to GTAC but apparently wont be fixed until NX10, so how are we meant to add test files to drawings?

 

 

Martyn, Snr CAE Engineer, Renishaw PLC
NX10 Tc10
6 REPLIES

Re: Note - Insert text from file

Gears Phenom Gears Phenom
Gears Phenom

I reported that one to GTAC a few weeks ago.

 

My work around, is to open the note file in a seperate editor, and copy-paste into my NX note.

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: Note - Insert text from file

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@$!#!%$#!!! 

 

I would hope they fix this in an MP!

 

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Note - Insert text from file

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Verified problem in NX9.0.3 (base and mp1).

 

Fixed in NX9.0.3 mp2.

Re: Note - Insert text from file

Gears Phenom Gears Phenom
Gears Phenom

Any unofficial off the record rumor on when NX9.0.3 mp2 will be available?

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: Note - Insert text from file

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor
Scheduled for November 7th.

Re: Note - Insert text from file

Valued Contributor
Valued Contributor

I have a work around now for this.

 

Text can be dragged and dropped from a Windows folder, so I have a journal that takes me straight to the required folder, then just drag and drop.

 

 

Martyn, Snr CAE Engineer, Renishaw PLC
NX10 Tc10