Cancel
Showing results for 
Search instead for 
Did you mean: 

Note difference in NX10 and NX11?

Builder
Builder

Hello, everyone,

 

I am doing titleblock update, linking a note to part attribute. I used NX11. So If I create a note in NX11, it shows a long window with various funtionalities in which I will go symbol->relation->insert Part attribute. 

 

Today, I moved back to NX10 (production use), I tried to do the same. But When I click the Note button, trying to create a note, there is just a "text to input" and specify location. No sysmol so that I can link to a part attribute.

 

Trying to find out is it some settings I should turn on to show these advanced commands? Thanks for any ideas!

Untitled.png

3 REPLIES 3
Highlighted

Re: Note difference in NX10 and NX11?

Builder
Builder
sorry. ..I assume it will be different role you turned on and actually it needs a restart of NX to see the effect...I did not know that

Re: Note difference in NX10 and NX11?

Honored Contributor
Honored Contributor

Did you try clicking the gear, in the upper left corner of the dialog, and see if that offers a "full" type menu option?

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: Note difference in NX10 and NX11?

Siemens Phenom Siemens Phenom
Siemens Phenom
On upper left corner of the dialog click on gear like icon and select option show more to see all available options within that dialog.

Regards,
Ganesh Kadole
#IngenuityIsNX | NX - What's New