Cancel
Showing results for 
Search instead for 
Did you mean: 

Nx 10 error

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Can anyone tell me what's this error and how to resolve this?
1 REPLY

Re: Nx 10 error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you have the syslog file, you can look in it to see if there is more data.

But most likely you have encountered an NX bug (or trying to do something that shouldn't be done).

If it is repeatable, you could file an IR with GTAC (or your VAR) to investigate the issue.

If you are running an API program or journal when it happens, the code probably needs to be fixed somehow.

You could search the Solutions database (https://solutions.industrysoftware.automation.siemens.com/) to see if anything resembles your issue.

 

Sorry, but it is a very generic error that doesn't help much in debugging the issue.

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled