Cancel
Showing results for 
Search instead for 
Did you mean: 

Nx 11 can be installed with 32 Bit Windows 8.1 Pro

Genius
Genius

Hello

 

I heard Nx 11 cannot be installed with windows 32 bit (Windows 8.1 Pro) we need 64 bit.

 

Is there any way to install Nx 11 and work with Nx 11 in 32 bit Windows Operating System.

 

thanks in advance

 

Sekar

3 REPLIES 3

Re: Nx 11 can be installed with 32 Bit Windows 8.1 Pro

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Sekars ,

 

Please find NX11 documentation: Operating system requirements

 

What I know is older versions of NX support 32 bit architecture. NX 9 or later versions are only supported with 64 bit.

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

Re: Nx 11 can be installed with 32 Bit Windows 8.1 Pro

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Sekars 

 


I heard Nx 11 cannot be installed with windows 32 bit (Windows 8.1 Pro) we need 64 bit.


As per NX 11 Operating system requirements,Minimum windows OS required are ""Windows 7 Pro and Enterprise editions (64 bit)"

 

Not sure about behaviour during or after NX installation on "Not Supported" platforms. Moreover, if there will be any issue, GTAC always use supported platforms/versions to replicate issues reported.

Re: Nx 11 can be installed with 32 Bit Windows 8.1 Pro

Valued Contributor
Valued Contributor

It's a 64 bit program. It can't run on a 32 bit OS. There is no 32 bit version of NX anymore.