Cancel
Showing results for 
Search instead for 
Did you mean: 

Nx help documentation error

Pioneer
Pioneer

I have 3 questions

1.is it possible to use NX 10 help documentation on NX 9?

2.I am getting java plug in error while searching any thing on help.

3.Is it possible to install help only on server so that all client can access the help by pressing F1?

7 REPLIES 7

Re: Nx help documentation error

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi

 

1. Possible but make no sense, use online help instead

https://community.plm.automation.siemens.com/t5/NX-Design-Forum/How-to-Locate-and-Access-NX-Help-Doc...

2. there is a patch available, or was, at GTAC

3. YES there is a Varaible available for it, you find it in the .env File something like UGDOC_BASE_DIR

 

 

Re: Nx help documentation error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

re 3:

UGII_UGDOC_BASE=http://your.server.here:8181

 

Port (8181) may change based on install on server  (I think Siemens changed the port at some point in time as well, I'm not sure if 8181 is the old or new port)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Nx help documentation error

Pioneer
Pioneer

thanks .

How to do the setting or configure each clients so that I can access the help from server and no need to install help files on each clients?

Re: Nx help documentation error

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

if i making a site environment for customers then i set al the customized stuff on a server and use a startup scrtipt that points to the customization.

 

Make a short cut to all the clients and it's done.


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Nx help documentation error

Solution Partner Legend Solution Partner Legend
Solution Partner Legend
Make a start script like nx10.cmd

@echo off

Set UGII_UGDOC_BASE=(path to help or online help)
Set UGII_Base_Dir=[Path to your Installation location, must be same on every client]

Set SPLM_LICENSE_SERVER=28000@[Servername]

Start [installation path or point with a variable] ugraf.exe. {example c:\siemens\ugii\ugraf.exe


I would recommend to use the online help

Re: Nx help documentation error

Solution Partner Legend Solution Partner Legend
Solution Partner Legend
It is depending which installer but it is 8282 knowerdays

Re: Nx help documentation error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you want all users to share the same NX configuration, I suggest you look at the "NXCustom" setup (see post at top of "NX Progrmaming & Customization" discussion forum for links to the appropriate version for you).

Read the top level "readme"

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled