Cancel
Showing results for 
Search instead for 
Did you mean: 

Nx8.5 fatal error

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Hello all,

After installing nx by one of my client whenever they are trying to open nx this is the error they are facing nx fatal error how to resolve this
6 REPLIES 6

Re: Nx8.5 fatal error

Legend
Legend

The error refers to NX9... while you specify NX8.5 in the title.

Is NX9 installed?

Do you use startup scripts?

Teamcenter installed? 

environment variables UGII_ROOT_DIR, UG_BASE_DIR

...

Frederik Verscheure
Evolve Consulting bvba
Freelance NX & Teamcenter consultant
frederik@evolve-consulting.be

Re: Nx8.5 fatal error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Did you get / look at syslog?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Nx8.5 fatal error

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
You are aware that there is Siemens GTAC for asking these sorts of questions? If you work for a reseller/solution partner (as I do), you should be directing these sorts of questions there, rather than asking the forums.
Anthony Galante, Senior Support Engineer
PhoenxPLM
24 versions of NX installed: NX4 to NX12, plus TC11.2

Re: Nx8.5 fatal error

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Sure. I will raise an IR.

Thank you all for ur valuable comments 😊

Re: Nx8.5 fatal error

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Will do that. Thanks Ken for your suggestion.

Re: Nx8.5 fatal error

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Sry I posted wrng picture.they installed 8.5 they are working on that particular issue.