Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

OD Thread Drafting Callout

Valued Contributor
Valued Contributor

Is there a way to insert a thread for an od thread like you can for a hole callout?

3 REPLIES 3

Re: OD Thread Drafting Callout

Legend
Legend

Hi @KUEI 

Yes

hole callout.jpg

Re: OD Thread Drafting Callout

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @KUEI ,

Hole Callout can be used for external threads as shown by @robot139 . Like drafting the same works in PMI application also.

Just FYI, In drafting there is a legacy command named "Feature Parameters" (use command finder - as it is a legacy command so hidden) which can also be used to display external thread dimension.

Re: OD Thread Drafting Callout

Valued Contributor
Valued Contributor

Thank you