Cancel
Showing results for 
Search instead for 
Did you mean: 

OFFSET A WRAP TEXT ON A CYLINDER BODY

Experimenter
Experimenter

DEAR ALL

I WANT TO MAKE AN OFFSET OF THIS TEXT WHICH IS WRAPED ON THIS CYLINDER FACE

model1.jpgWRAP TEXT ON CYLINDER

 

5 REPLIES

Re: OFFSET A WRAP TEXT ON A CYLINDER BODY

Phenom
Phenom

Why don’t you offset the face and wrap around that? Then you could use “Delete Body” to delete that offset body.

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: OFFSET A WRAP TEXT ON A CYLINDER BODY

Experimenter
Experimenter

i want to extrude that wrap text from that cylinder face

Re: OFFSET A WRAP TEXT ON A CYLINDER BODY

Siemens Phenom Siemens Phenom
Siemens Phenom

Use Divide Face to divide the cylindrical surface with the letters and then extrude the small faces inside each letter.  You could also look at the Emboss and Offset Region commands.

Regards, Ben

Re: OFFSET A WRAP TEXT ON A CYLINDER BODY

Phenom
Phenom

Check the attachment. I couldn’t find an easy way but a bit of labor intensive and manual method.

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: OFFSET A WRAP TEXT ON A CYLINDER BODY

Siemens Phenom Siemens Phenom
Siemens Phenom

And if you have the license, there's always Global Shaping.  You can extrude text in a single command on a planar surface and use draft.  Global Shaping then maps the extruded text on to any surface you desire, not just cylindrical.  See attached.

 

Ben

global_shaping.png