05-27-2016 01:40 AM - edited 05-27-2016 09:47 AM
05-27-2016 09:12 AM
Use the "Object Attribute Management" dialog in MoldWizard.Be sure object type is set to part, not component. That's how you end up with both.
o
w
05-27-2016 09:56 AM
After use "View manager" and show only A side parts, NX show all parts with attribute MW_Side=A.
I have same parts on both side,and are show, when check "mold fixed half", this parts show, but belong to the B side. Another solution?
05-27-2016 10:27 AM
Using the dialog I posted above, you will need to change the attribute to side you want. Open the Object Attribute Management dialog , select the object that you want to change, and where it says value, click on it and you can change it.Then click the circled icon, and it will add/update that attribute to whatever you have selected. whatever you have selected.
05-29-2016 10:30 AM
Once again. I have 4 same parts in assembly , 2 on A side and 2 on B side. In object attribute management, select attribute MW_Side=B and add to part.
In view manager hide A side an solution:
2 parts belong to A side is allways visible. After hide B side, all 4 parts is hidden.
05-30-2016 08:39 AM
There are some limitations: One component could have only one False body=one mounting option. Same way each could have only one location/parent assembly. E.g. Same screw has to have different filenames to be displayed accordingly. I’ve submitted ER on this.
So I think you have to use “Make Unique” and rename your components even they are same.
05-31-2016 11:51 PM
It is not a good solution for my bill of material. In my assembly is 26 types screw (but 50 files).I do not see which are the same (filename screw01, screw02, screw03, ...).Is possible implement size of screw in to filename, or name of component?
06-01-2016 02:20 PM - edited 06-02-2016 07:53 AM
It’s how NX programed to work. If you don’t agree, you may submit your concerns and register some ERs as I did. May be they will consider it one day.
By RMB, a library component, it’s possible to edit it(filename=Screw01) to become any type of a screw. If File name is to contain the screw size, then there will be constant file creation happening. But I’ve seen this (file name designates by the screw size) working quite efficiently in other software.
So in NX, you have to see file attributes to find the screw properties.