Cancel
Showing results for 
Search instead for 
Did you mean: 

OmniCad Addon for NX10

Valued Contributor
Valued Contributor

Has anyone used the OmniCad addon in NX10? I have tried to run the sentinal installer in order to use the OmniCad addon in NX10 without success. Is this an addon that requires an additional license?

Michael Pinto | Designer
NX11|Windows 10 Enterprise 64bit|HP Z-Book Studio G3 Workstation|Intel XEON E3-1505M|32GB Ram|Nvidia Quadro M1000m w/4GB
5 REPLIES

Re: OmniCad Addon for NX10

Siemens Legend Siemens Legend
Siemens Legend

Yes. You need an additional license.

In Italy Omnicad addon is sold directly by Omnicad people.

I'm a good friend od Omnicad guys... if you need any information, please let me know: I can put in touch with them.

Beppe G
Siemens PLM Italy

Re: OmniCad Addon for NX10

Genius
Genius

What does OmniCad do exactly? is it similar to Shape Studio/Realize Shape?

Re: OmniCad Addon for NX10

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

OmniCad is morphing software and is extremely powerful. Likely more along the lines of progressive die desgin and springback correction for mold as it works on surfaces not solids.

NX Free Style on YouTube

 

Re: OmniCad Addon for NX10

Experimenter
Experimenter

Hello! 

    I was using the Demo Lic and the Omnicad was enable several days ago.But it currently becomes disabled today. (Not just my computer but also my colleagues' )When I click the MeshTransformer or other function, my NX will crush.I just cannot figure out what happened. Please help me, thanks.

Re: OmniCad Addon for NX10

Siemens Phenom Siemens Phenom
Siemens Phenom

if you have a problem with you license please contact the hotline.

Steve V