Cancel
Showing results for 
Search instead for 
Did you mean: 

Operation Navigator Columns

Pioneer
Pioneer

Hi All,


I am customising the Operation Navigator Columns columns using NX-Open and have the following issue.

 

Problem:

Currently I can manually customise the columns to my requirement, but when the session closes, the information columns are reset.
I would like to retain the information so that I don't have to customise manually every time.

 

Question:
Does NX store the column inormation in any file/registry?
If yes, Where can I find the file which NX uses at launch to set default columns.

 

Thanks for your time.


Regards,

Faisal

2 REPLIES

Re: Operation Navigator Columns

Master
Master

Save a role and this should save them.

Shags72 Mfg. Eng.
Windows 10 Pro 64bit
NX 11.0.2.7 MP2 Teamcenter 11
Dell M7720 i7-6820HQ 16GB RAM,
NVIDIA Quadro P3000

Re: Operation Navigator Columns

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You better ask this in the manufacturing form, since this is not a question related to modeling or drafting.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide