Cancel
Showing results for 
Search instead for 
Did you mean: 

Ordinate dimension - redefine margins

Builder
Builder

How to redefine margins in ordinate dimension in NX9?

In help is - see image, but not work.

4 REPLIES

Re: Ordinate dimension - redefine margins

Siemens Phenom Siemens Phenom
Siemens Phenom

Here are the instructions in the Help:

 

To move an ordinate origin:

  1. Double-click a dimension in the set to open the Ordinate Dimension dialog box in the edit mode. 

  2. In the References group, click Select Origin .

  3. Select the new origin point.

  4. Click Close.

     

    The origin moves and all of the dimension values are recalculated from the new origin.

Re: Ordinate dimension - redefine margins

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

double click one dimension.

the ordinate dimension dialog box pops out.

you should see a broken line in the graphics window, see the image for reference. here I have vertical and horizontal margin.

i marked it with a blue pen.

margin.JPG

 

rightclick one of the broken lines, and select move margin. (in my case i choose the vertical one)

margin.png

 

change the value of your offset to the value that you need.

that would move your first margin and do the same on the other one.

 

hope this helps

 

Re: Ordinate dimension - redefine margins

Builder
Builder

Thank You Jahnsen, now it works.

It would be better if the margin was highlighted (as the NX85).

Re: Ordinate dimension - redefine margins

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

welcome! Smiley Happy