Cancel
Showing results for 
Search instead for 
Did you mean: 

Overlay CGM failed.

Creator
Creator

Hello All.

 

I am getting an error, when I tried to Overlay the CGM

 

Error "Overlay CGM failed".

 

I have already created Snapshot Data and saved the part, After opening it again and made some changes in the modeling and updated the drawing. then I tried to Overlay CGM using the option from Track Drawing Changes. I am getting an error " Overlay CGM Failed".

 

Can anyone point me, where the error is happening.

2 REPLIES

Re: Overlay CGM failed.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Have you looked in the syslog?

(help -> [NX] Log File)

 

There may be more info in there.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Overlay CGM failed.

Creator
Creator

Hello Ken.

 

I have checked syslog, This is what, has been logged in Syslog.

 

>>>> Error code 735004 caught in file "o:\ugnx1001\ip4\src\ugui\no\ind\uigblfunc.c" at line number 594

>>>> Error code 735004 caught in file "EVTLoop.cpp" at line number 1751

>>>> Error code 735004 caught in file "o:\ugnx1001\ip4\src\ugui\no\ind\uigblfunc.c" at line number 397

>>>> Error code 735004 caught in file "o:\ugnx1001\ip4\src\uginitint\no\ind\clink.c" at line number 715

&MACRO FOCUS CHANGE IN 1

&MACRO MESSAGE_BOX -2, Overlay CGM failed.

 

Any suggestions....