Cancel
Showing results for 
Search instead for 
Did you mean: 

'PART IS REFERENCE ONLY '

Experimenter
Experimenter

IN DRAFTING MODULE MODEL USED FOR DRAFTING  IS SHOWN AS   'PART IS REFERENCE ONLY '. IS THERE ANY WAY TO CHANGE THIS WITHOUT EFFECTING THE DRAWING. IM USING NX 7.5 STAND ALONE.Capture.JPG

6 REPLIES

Re: 'PART IS REFERENCE ONLY '

Builder
Builder
Hello@manulal,

in this case i think its not possible,,if you have to change the drawing,,,you have to modify the object part,,,



thanks
Warm Regards
Thomas Roman
Machine Designer

Re: 'PART IS REFERENCE ONLY '

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Manulal,

 

There is command 'Replace Component' in NX 8 and I hope that it will also be available in NX 7.5. But you can not replace a component with another having same name. There is no simple way to do this.

 

With some rework depending upon your drawing, you can make "DETAIL_A" as displayed part. Create a new drawing part with reference to the "DETAIL_A" then copy paste the drawing from "DETAIL_A_DWG" to the new drawing part in the drafting.

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

Re: 'PART IS REFERENCE ONLY '

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @Manulal,

 

The "Part is Reference Only" status can only be changed in a Teamcenter managed session of NX via the "Component is Reference-Only" checkbox on the Component Properties dialog:

 

Screenshot - 6_13_2017 , 9_09_44 AM.png

 

This is independent of the component being a "drafting component" as indicated in the Assembly Navigator as an icon with a yellow block with a drawing sheet in the background.  When checked, the "Component is Reference-Only" checkbox removes that component from the BOM in Teamcenter (in newer versions adding a view of a part, (a.k.a. drafting component) also checks "Component is Reference-Only", but it can be disabled afterwards).

 

What is it that you're trying to do that you believe "Part is Reference-Only" is affecting you?

 

Regards, Ben

Re: 'PART IS REFERENCE ONLY '

Gears Phenom Gears Phenom
Gears Phenom

In Native NX you would have to set the attributes:

PLIST_IGNORE_MEMBER

PLIST_IGNORE_SUBASSEMBLY

to have it be ignored in the BOM, aka Parts List

 

Could be the attribute REFERENCE_COMPONENT is set?  ref IR 7798551

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: 'PART IS REFERENCE ONLY '

Experimenter
Experimenter

Its not effecting anything in our side, but our client want the drawings to be with out reference parts in the drawing. I tried coping, exporting,replacing, nothing was sucessful.

 

 

Re: 'PART IS REFERENCE ONLY '

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

In this case the part is added later on the drawing and not in an good way wat you normall do when working in Master model Drawings.

So this part is just added in the drawing as reference.

 


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions