Cancel
Showing results for 
Search instead for 
Did you mean: 

PDW assembly navigator structure

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi everyone, 

 

I need to help in PDW. How I can control assembly navigtor structure. Can I change the position of parts in nawigator by some template?str001521.png

 

best regards

lukipap

3 REPLIES

Re: PDW assembly navigator structure

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,
Do you mean to reposition a part from one node to another (from one subassembly to another) in ANT???
I don't have much PDW know how but it will break the wave links in the part for sure (which i guess are creaated on the fly in PDW).
If you just want to reorder the part in assembly navigator then that can be done using attributes (sort using attributes).
One such discussion is given below..
https://community.plm.automation.siemens.com/t5/NX-Design-Forum/Assembly-Structure-Modification-in-p...
Regards
Kapil

Re: PDW assembly navigator structure

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

The screenshot indicates that you are currently using the "chronological" order; the system also defines an "alphabetic" and "alphanumeric" order. If you would like a custom order for the components, you can create your own by dragging the components into the desired order and saving the custom order. You can change between the available orders by right clicking on the top level assembly (in the navigator) and choosing "navigator order".

 

https://docs.plm.automation.siemens.com/tdoc/nx/11/nx_help/#uid:xid617396

Re: PDW assembly navigator structure

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
but I mean only the structure of Proresive Die Wizard