02-01-2017 08:50 AM
I cant do a save as or a save. but I can export, so it's not a total loss.
I've never seen this error before, kind of hard to send the file into Gtac when I cannot save it.
NX 11.0.1.11 on win7
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies
Production: NX 12.0.2 / Autoform r7 /WorkNC 2018 r2
Testing:NX EAP
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro
02-01-2017 10:52 AM
Hello @R_Newcomb,
Sending the file would indeed be hard
But sending the NX syslog could be very useful. This might give more insight on the problem even without the Part. So I would still submit the file to GTAC, possibly with the last step you performed before the problem arose.
Kind regards,
02-01-2017 11:51 AM - edited 02-01-2017 11:51 AM
sent in the IR, the previous save was about 30 min in, I remember cause to just canceled my save timer without trying to save.
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies
Production: NX 12.0.2 / Autoform r7 /WorkNC 2018 r2
Testing:NX EAP
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro