Cancel
Showing results for 
Search instead for 
Did you mean: 

PLOT A CURVE ON UNEVEN LENGHT OF A SURFACE

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello everyone,

 

 

  i have a query regarding plotting a curve onto an uneven surface with uneven widhts from start to end and my question is there anyway to plot a curve exactly or almost equal to its center on the surface of the curve or ayother ways of doing it??curve.JPG

 

 

 

Any suggestions can help!

 

 

 

Thanks

1 REPLY

Re: PLOT A CURVE ON UNEVEN LENGHT OF A SURFACE

Siemens Phenom Siemens Phenom
Siemens Phenom

If the surface is untrimmed then a couple of options:

Isoparametric curve - set number of curves to 3, use the middle curve

Enlarge Surface - set the u or v to 50%, use the edge of the new surface

 

Steve V