Cancel
Showing results for 
Search instead for 
Did you mean: 

PMI Center Mark in detailed view on drawing

Experimenter
Experimenter

Hello guys, 

 

I have a problem with PMIs in NX 11.

I need to transfer PMIs to a drawing. Is there a way to "break" a PMI center mark in a detailed view? Because I only need one part of the center mark and the actual center will be way out of the detailed view (see screenshot).

 

2018-03-24 07_14_37-NX 11 - Drafting - [C70213832_A;1-- (Modified) ].jpg

 

 

Unfortunately I can't find a way to limit the display to the actual view boundary.

A simple centerline would help but there is no geometry to display it in this view.

 

Is there any way to solve this issue?

 

Cheers

Dominik

4 REPLIES 4

Re: PMI Center Mark in detailed view on drawing

Siemens Phenom Siemens Phenom
Siemens Phenom

@Dominik79

After placing the view on the drawing and inheriting the PMI center line, you should be able to define the view boundary using a manual rectangle as in the movie below.

(view in My Videos)

Regards,
Abe

Re: PMI Center Mark in detailed view on drawing

Experimenter
Experimenter

hello @Abeinjapan,

 

 

thanks for you reply. But this won't help in this case.

 

I assume you used the view settings PMI->From Model view?

 

I have to use

PMI-> Align to Drawing (show PMI on drawing), as the PMI dimensions need to be placed over and outside of the view boundaries (detailed view borders).

 

In this case the PMI Center Mark wont be cut off. That's my exact problem.

 

Any other idea? Smiley Happy

 

Cheers

Dominik

Re: PMI Center Mark in detailed view on drawing

Siemens Phenom Siemens Phenom
Siemens Phenom

@Dominik79

The only thing I can think of that's not a particularly elegant solution would be to hide (don't inherit, blank or move to hidden layer) the inherited center mark and then create a new 2D centerline to the appropriate size by selecting available control points from the extracted edges.

(view in My Videos)

Regards,
Abe

Re: PMI Center Mark in detailed view on drawing

Experimenter
Experimenter

ah, that's unfortunate, but it's a way Smiley Happy

 

thanks for your help