Cancel
Showing results for 
Search instead for 
Did you mean: 

PMI datum feature symbol unable to attach leader to datum plane

Experimenter
Experimenter

I spoke with Mr. John Baker in a forum of ENG-tips and he suggested that I reach out on this site to have an "ER" opened for this issue we discovered with NX9.  The problem is simple...our designers are unable to attach the leader of a PMI datum feature symbol to an actual datum plane.  The current work-around is to create a line and attach the symbol to it.  I am unfamiliar with GTAC and "ER"s so any guidance on how this problem can be reported properly would be greatly appreciated.  Thank you.

3 REPLIES

Re: PMI datum feature symbol unable to attach leader to datum plane

Siemens Phenom Siemens Phenom
Siemens Phenom

This is not a venue to open a formal ER.  You need to call GTAC and have them open the ER for you.  For information about how to contact GTAC, go to:

 

https://support.industrysoftware.automation.siemens.com/gtac.shtml

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: PMI datum feature symbol unable to attach leader to datum plane

Experimenter
Experimenter
So is there some solution regarding the problem described in the topic?
I am using NX10 and also not able to attach Datum Feature Symbol leader to a plane.

Re: PMI datum feature symbol unable to attach leader to datum plane

Siemens Phenom Siemens Phenom
Siemens Phenom
ER 7898217 was submitted against NX10 requesting the ability to attach a Datum Feature Symbol to a Datum Plane. You can contact GTAC and request that you're notified when this ER is implemented.

Regards, Ben