Cancel
Showing results for 
Search instead for 
Did you mean: 

PMI_not_Shawn_In_Drafting

Builder
Builder

hello NX Experts,

i have a query with nx drafting,

I added Feature dimension as PMI but
i cant get Feature PMI dimension in drafting view

and one more thing , i wanna adjust that dimension in view , recently i cant adjust that feature PMI dimension also , i thing after adjustment i can see.....

EG. i attach image file , in that i added Feature as PMI dimension in model ,but i cant get it in Side view, i also set drafting in reference = PMI from model view ,Entire part, show only bla bla

how to get that PMI dimension in Drafting view ,

any body have idea for it!!!!!!!

 

 

Capture_Extrude_dimension.JPGModel viewCapture_Extrude_dimension_D.JPGDrafting view

 

 

 

 

 

 

 

 

Warm Regards
Thomas Roman
Machine Designer
3 REPLIES 3

Re: PMI_not_Shawn_In_Drafting

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

Try this please.

 

pmi_1.jpg

 

pmi_2.jpg

Highlighted

Re: PMI_not_Shawn_In_Drafting

Siemens Creator Siemens Creator
Siemens Creator

The above information will make the PMI visible in the modeling views.

 

To view the PMI in drafting views, you need to check/set the PMI properties of each view to allow PMI.

 

This is modeling data with two curves, a PMI NOTE and a PMI dimension.

2016-10-04 09_13_19-NX 11 - Modeling - [nx11_spline_length_dim.prt].jpgMODELING

 

Here is the DRAFTING data - using the SETTINGS for a view.

 

2016-10-04 09_13_04-Program Manager.jpgDRAFTING

Dave Figurski

GSS / Siemens Industry Sector

Re: PMI_not_Shawn_In_Drafting

Builder
Builder

thank for help @ kapilsharma & qztjv4

 

got the solution

Warm Regards
Thomas Roman
Machine Designer