10-04-2016 06:56 AM - edited
hello NX Experts,
i have a query with nx drafting,
I added Feature dimension as PMI but
i cant get Feature PMI dimension in drafting view
and one more thing , i wanna adjust that dimension in view , recently i cant adjust that feature PMI dimension also , i thing after adjustment i can see.....
EG. i attach image file , in that i added Feature as PMI dimension in model ,but i cant get it in Side view, i also set drafting in reference = PMI from model view ,Entire part, show only bla bla
how to get that PMI dimension in Drafting view ,
any body have idea for it!!!!!!!
Model view
Drafting view
Solved! Go to Solution.
10-04-2016 07:40 AM
Hi,
Try this please.
10-04-2016 09:18 AM
The above information will make the PMI visible in the modeling views.
To view the PMI in drafting views, you need to check/set the PMI properties of each view to allow PMI.
This is modeling data with two curves, a PMI NOTE and a PMI dimension.
MODELING
Here is the DRAFTING data - using the SETTINGS for a view.
DRAFTING
10-05-2016 03:40 AM
thank for help @ kapilsharma & qztjv4
got the solution