Cancel
Showing results for 
Search instead for 
Did you mean: 

.POD file not displaying in NX 11

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello All,

 

I am trying to import a point cloud into NX however there is no display. I have have used the fit command to confirm the file is centered and went through the show/hidden tabs to make sure the view is enabled.

 

Capture.PNG

 

I am selecting the Reference Point Cloud

 

Capture1.PNG

 

Then I select the file I wish to import.

 

Capture2.PNG

 

Then after clicking load points now and clicking ok, you can see the model has been loaded from the part navigator but nothing was displayed.

 

I think I need to enamble some feature but I can't seem to find where.

 

Many thanks

4 REPLIES

Re: .POD file not displaying in NX 11

Honored Contributor
Honored Contributor

Did you press the "load points now" button in the dialog? If not, try expanding the point cloud folder, right clicking on the point cloud, and choosing "load points". If you still don't see anything, it might be a layer setting (the points are on an invisible layer) or the points might be outside the view clipping bounds.

Re: .POD file not displaying in NX 11

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Yup, I clicked the load points button between picture 2 and 3

Re: .POD file not displaying in NX 11

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
What is there standing in the "Point clouds" folder in your part navigator?


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: .POD file not displaying in NX 11

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

The name of my file, called MyFactory

 

 

Capture.PNG

 

However, I was working in a Virtual machine at the time and tried the same steps within my Native NX. There is works fine. There must be something wrong with my virtual machine rendering or something.