Cancel
Showing results for 
Search instead for 
Did you mean: 

.PRT OPEN IN MODELING

Valued Contributor
Valued Contributor

Is there a way to get a .PRT file to open directly in the modeling app when I click on the file?

12 REPLIES 12

Re: .PRT OPEN IN MODELING

Phenom
Phenom
The .prt file will open the application it was last saved in. So open the file, start modeling, and save it.

You might also have to make sure file associations are set to start NX. For example, if Creo was installed after NX, file associations will be set to try to open the .prt file in Creo.

Re: .PRT OPEN IN MODELING

Valued Contributor
Valued Contributor

Whenever I click on the prt file the main NX page opens. The file itself does not open. Once NX is open I must either drag the file to NX, or select open and pick a file.

Re: .PRT OPEN IN MODELING

Siemens Phenom Siemens Phenom
Siemens Phenom

Are you double clicking on .prt file? Generally, what I know is file is opened in software/program you've associated it with.

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

Re: .PRT OPEN IN MODELING

Valued Contributor
Valued Contributor

Yes, I am.

Re: .PRT OPEN IN MODELING

Siemens Phenom Siemens Phenom
Siemens Phenom

This post might be helpful to you: Open part file by double click

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

Re: .PRT OPEN IN MODELING

Valued Contributor
Valued Contributor

Link on that page is not available Smiley Sad

Re: .PRT OPEN IN MODELING

Siemens Phenom Siemens Phenom
Siemens Phenom

Do you have Web Key account? Try logging into that page.

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

Re: .PRT OPEN IN MODELING

Valued Contributor
Valued Contributor

I will have to ask someone. Not even sure what it is.

Re: .PRT OPEN IN MODELING

Siemens Phenom Siemens Phenom
Siemens Phenom

Q: How to open part file in required version of NX by double click?

Solution:

In order to correctly associate .prt file to NX use an external tool like
'Defaults Program Editor', since manual editing of the Windows registry is
rather difficult.
Download that tool here http://defaultprogramseditor.com/ : it is a simple
tool, it doesn't need any installation (just a .exe to launch when you need
it). 

After downloading it just run the executable and follow these main steps.

01) Select "File Type Settings"
02) Select "Context Menu"
03) Select ".prt" extension > Next.
04) Select "Edit Selected Command..."
05) Select "Browse" to specify the path of "ugs_router.exe". It will be
available at %UGII_BASE_DIR%\UGII\ugs_router.exe
06) Select "Open".
07) Complete the Program path entry by adding these ones (-ug -use_file_dir
-version=V25.5 "%1" , where -version=V25.5 identifies NX7.5).
   Following are the versions of NX:
   v25.5=NX7.5
   V26.0=NX8
   V26.5=NX8.5
   V27.0=NX9

   For e.g. the complete line of "Program path" will look like this
("E:\Siemens\NX75\UGII\ugs_router.exe" -ug -use_file_dir -version=V25.5 "%1").
08) Select "Next"
09) Select "Save Context Menu" > OK.
10) Close the "Default Programs Editor" dialog.
11) Double click on the NX part file and now it will open in the set version of
NX i.e. NX7.5

 

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!