Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: .PRT OPEN IN MODELING

Valued Contributor
Valued Contributor

If ugs_router.exe is the executable to open router, when is the exe to open modeling?

Re: .PRT OPEN IN MODELING

Siemens Phenom Siemens Phenom
Siemens Phenom

Sorry I'm unaware of it.

This post might be helpful to resolve your issue: Unable to launch NX 9.0 from Explorer

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

Re: .PRT OPEN IN MODELING

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

ugs_router doesn't open the routing module.

It is used (depending on ???) to find an existing NX session & use that, instead of always opening a new session (useful in a Teamcenter environment)

It (indirectly) calls ugraf.exe, which is the main NX executable (which can then be used for modeling, drafting, CAM, routing, etc. as your license file allows)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled