Cancel
Showing results for 
Search instead for 
Did you mean: 

Pack And GO

Experimenter
Experimenter

is there any option in NX similar to "Pack and go"  Option in Solidworks?...

3 REPLIES 3

Re: Pack And GO

Phenom
Phenom

Hi @KA,

not as OOTB (Out of the box) integrated into NX, but you have to customize your toolbar with a journal called Zip Assembly.

You can find all files in the zip on this thread.

Thank you...

Using NX1859
RuleDesigner PDM

Re: Pack And GO

Legend
Legend

The last post in this thread has a link to an NXzip. that uses 7zip 

 

I still use UGzip more often out of habit though as its right in my File->Export menu ( using NXcustom)

Rob Newcomb, CAD/CNC/Simulation manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r8 /WorkNC 2019 r1
Testing:NX 1855
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro

Re: Pack And GO

Phenom
Phenom

Menu==>Assembly==>Cloning

 

This is a very basic of “Pack and Go”. Go through the tabs and you may find Naming Rules etc.

 

Unfortunately, if you have master model drawings, they have to be picked manually.

 

If you need any further help, just provide me a sample.

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW