Cancel
Showing results for 
Search instead for 
Did you mean: 

Paint a Threaded hole with yellow color Automatitly

Hello guys

 

I want to paint a Threaded hole with yellow color automatitly

 

Capture Hole.PNG

 

Another issue is:

 

Is it posible to make a threaded hole without dashed line wich represents the nominal dimension

I prefer that the nominal dimension can be represent as the following picture:Capture Hole-2.PNG

 

 

7 REPLIES

Re: Paint a Threaded hole with yellow color Automatitly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@FrankSwinksposted some journal code here that may be a good starting point for coloring hole faces.

Re: Paint a Threaded hole with yellow color Automatitly

Experimenter
Experimenter

First off, how are you making these holes?

 

If you use the Moldwizard pocket command, you can change the colour of the surfaces of the template model that make the hole, by default these are o layer 99 and reference set false. You may then need to change the modeling preferences so that the hole surfaces will inherit the template surfaces properties.

 

Another way is to select the feature either on the model or in the part navigator and part history, right-click-mouse and you have the option  'Assign Feature Color'.

Re: Paint a Threaded hole with yellow color Automatitly

Soo Good cowski1
Thank you!!!

Re: Paint a Threaded hole with yellow color Automatitly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

As to modeling the thread major diameter as the "hole" diameter - you can do this with a UDF (user defined feature).

Short of doing that, maybe use counterbore hole, and set the cbore dia & depth as appropriate for the thread.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Paint a Threaded hole with yellow color Automatitly

Good!!!
Thank you

Re: Paint a Threaded hole with yellow color Automatitly

I didn't Know that kind of tool but it's a good idea

Paint a Threaded hole with yellow color Automatically

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer