Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Part Cleanup Batch

Valued Contributor
Valued Contributor

Does anyone know if it's possible to run Part Cleanup as a batch run outside of NX?
Is there an external EXE file for that function that could be run on a folder or group of parts native and/or within Teamcenter?

PartCleanUp.png

3 REPLIES

Re: Part Cleanup Batch

Genius
Genius
Depending on your license you can create a NX Open application to do it. Or you make a journal and uses "run_journal" in batch mode.

Re: Part Cleanup Batch

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The refile_part utility has an option for part cleanup; but the automatic cleanup is fairly limited compared to the options offered in interactive NX. Alternately, you could create a journal of the part cleanup options that you want. If you have an author license, you can compile your own .exe for a "batch" run. If you do not have an author license, you can use the run_journal utility to get a similar result. However, the journal code (wheter run as a journal or compiled to .exe) will require the use of an NX license while it is running.

Re: Part Cleanup Batch

Valued Contributor
Valued Contributor

I'll look into trying those. I haven't used the run_journal utility or built an NX open application so I'll need to read up on how to get that created. Thank you all for the advise.