Cancel
Showing results for 
Search instead for 
Did you mean: 

Part Cleanup Function

Genius
Genius

Using the part cleanup utility with the Delete All Materials selected...

Does this remove all the materials from the model even if they are assigned or just the materials that are not assigned?

 

I tried using it and it doesn't appear to remove any materials assigned or not assigned.

Using NX 9

PartCleanup.png

materials.png

5 REPLIES 5

Re: Part Cleanup Function

Siemens Phenom Siemens Phenom
Siemens Phenom

On the Customer Defaults-> Gateway-> Materials/Mass-> Attributes tab there are some settings which control automatic creation of part and object attributes when materials are assigned.

When the materials are deleted from the part with part cleanup, these automatically created locked attributes will remain.  If you do not want them, then you would have to turn off the customer default which controls their creation.

If you have parts which already have these locked attributes and you want to clean them up, then you would need to:
- change the titles used by the Materials module on this same tab
- turn ON Customer Defaults-> Gateway-> User Attributes-> Security-> Attribute Locking via NX Open
- write an API program to unlock and then delete the Material attribute

 

If you have require further information, you will need to contact GTAC.

Re: Part Cleanup Function

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I might be wrong, but I believe that "Delete all Materials" refers to visualization materials (materials and textures applied for renderings) rather than physical property materials assigned to solids.

Re: Part Cleanup Function

Genius
Genius

That would make much more sense than the actual material properties given the other options around that check box.

 

RonY, given your explanation on how the Material properties get locked are you saying that the Part Cleanup is for the material properties and not the Render Materials?

 

Thank you both for replying!

Re: Part Cleanup Function

Siemens Phenom Siemens Phenom
Siemens Phenom
It deletes all materials and textures applied to a part.

This only applies to unlocked material attributes.

The locked attributes are applied to files depending on the settings in customer defaults.

Ron Young
Prod Driven Svs

Siemens Industry Sector
Siemens Product Lifecycle Management Software Inc.
13690 Riverport Drive
MARYLAND HEIGHTS, MO 63043 United States
Tel. :+1 (314) 264-8811
Fax :+1 (314) 264-8906
young.ronald@siemens.com
www.siemens.com/plm

Re: Part Cleanup Function

Genius
Genius

Perfect! Thank you so much!