Cancel
Showing results for 
Search instead for 
Did you mean: 

Part Cleanup error

Creator
Creator

When using Part Cleanup on some parts i am getting an error message.

"  A deleted or invalid class id was used  "

I have tried unsucessfully to use a smaller and smaller subset of the Part Cleanup settings to try and isolate the issue.

What is causing this ?

NX 11.0.2.7

9 REPLIES

Re: Part Cleanup error

Siemens Phenom Siemens Phenom
Siemens Phenom

What options are you selecting in the part cleanup dialog? What data do you need to clean? To which application does it belong.. modeling, assembly, drafting? Could you please mention some more details.

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

Re: Part Cleanup error

Creator
Creator

This is in Modeling and this particular part has one body imported from a step 214 with no features added.

Cleanup is being run as a precaution, this part exhibits no other problems.

Re: Part Cleanup error

Siemens Phenom Siemens Phenom
Siemens Phenom

You can review the log file for the error. Did you try this on another machine or NX version?

Can you upload that part here? Because I got the same error with some particular steps/process related to PMI.

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

Re: Part Cleanup error

Creator
Creator

cannot upload file but i have uploaded the log.

The error does not occur on another machine but then reocurrs om my machine.

The log shows an error that I wonder may be pointing to an installation error?

Re: Part Cleanup error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The log file shows that you are using NX 11.0.2.7 MP3. Is the other computer (the one that does not error) at the same patch level?

Re: Part Cleanup error

Creator
Creator

No it is  NX 11.0.2.7 MP4

Re: Part Cleanup error

Creator
Creator

I have installed NX 11.0.2.7 MP4 now but error persists

Re: Part Cleanup error

Creator
Creator

This was submitted to GTAC and is now

PR 9033759; Desc: Part Cleanup Error: A deleted or invalid class id was used

Re: Part Cleanup error

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor
The problem was found to be a rogue empty group created when the STEP data was imported. The group can be manually deleted via the Part Navigator. Development are going to determine why Part Cleanup raises the error and is not able to delete the empty group.

Regards, Ben