Cancel
Showing results for 
Search instead for 
Did you mean: 

Part Familiy with Expressions usage of If and then

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello Folks,

 

i had to create a part with several openings witch i control with "Suppresed by Expressions" No i got the situation that i need some logic in it. Example.

 

If Opening 7 is active two other openings must be suppressed. With Expressions it works fine. BUT i would to this in the part Family. But i can select the expressions with  if and then.


I Also tried to pack them in an other expression but the inteligence of NX recognized it also. I tried to do in Excel but won´t work also.

 

IS it possible to do or not? Tried with NX10 , NX11, NX11 Daimler

7 REPLIES

Re: Part Familiy with Expressions usage of If and then

Siemens Phenom Siemens Phenom
Siemens Phenom

What if you use 'Features' with YES/NO values. 

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

Re: Part Familiy with Expressions usage of If and then

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi Ganesh,

thx for the idea. The Problem is i organized all in feature Groups. The Part Family only recognizes the features itself and no groups. I have 72 Features and with the goups i only need to control 8 "Features".

 

call_1.jpg

Re: Part Familiy with Expressions usage of If and then

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello,

 

Feature Groups are also avialable if you work with Part Families. Supress-Feature.JPG

 

The Feature Group could also be supressed with an expression

 

Supress-Feature_2.JPG

 

Hope that helps or did i get you wrong?

Re: Part Familiy with Expressions usage of If and then

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi Andre,

 

you are right. the feature groups are also available... i dont know why i did not see them before but they are there...

 

but it makes no difference for me because if and then is not working... or also did not see it

 

And the accept as solution was not correct klicked by me.. sorry

 

i neet to control the feature groups with if and then thats my problem. IF Opening 7 is available then opening 2 and 3 must be blanked automatically..

Re: Part Familiy with Expressions usage of If and then

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

IF-conditions could also be used in this way for example :

 

Supress-Feature_3.JPG

 

Supress-Feature_4.JPG

 

Kind regards,

Andre

Re: Part Familiy with Expressions usage of If and then

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

then i dont know what i did wrong.... 

 

i will check all and give feedback

Re: Part Familiy with Expressions usage of If and then

Solution Partner Legend Solution Partner Legend
Solution Partner Legend
ok i understood how you did that. you made yourself an expression and then you asked for that ... ok... other way i wanted it but soultion for me thx