Cancel
Showing results for 
Search instead for 
Did you mean: 

Part attributes not shown on the drafting sheet

Creator
Creator

Hello All,

I have recently started using NX10.

I have carried forward all the drafting templates I had from NX8.5. 

The templates have the title block filled and linked with the part attributes. 

Now in NX10 if I open the template file the title block is filled but if I try to draft a designed part the title block comes up to be empty. Any help is really appreciated. 

 

Thank you

Naga

2 REPLIES 2

Re: Part attributes not shown on the drafting sheet

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
I think that the way that the attributes are linked into the title block changes in either NX9 or NX10. Our video on drafting attributes covers some of what you are after: https://vimeo.com/album/3065578/video/100179684
Anthony Galante, Senior Support Engineer
PhoenxPLM
24 versions of NX installed: NX4 to NX12, plus TC11.2

Re: Part attributes not shown on the drafting sheet

Creator
Creator

I had to map the model templates too. Then it was fixed.