Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Part family component and assy constraints

Gears Phenom Gears Phenom
Gears Phenom

NX9 and TC 10.

 

If I have a part family component, and I replace the component with another family member, the assy constraints should stay associative, correct?  The only change in the family members, is a hole location, same hole, just a different location, yet when we swap, the constraints are blowing up.

 

I have not dug too deep yet, but my understanding is that they should just keep working.

 

-Dave

-Dave
NX 11 | Teamcenter 11 | Windows 10
6 REPLIES

Re: Part family component and assy constraints

Siemens Phenom Siemens Phenom
Siemens Phenom

Based on how you've described the workflow I would have to agree with you, it should work OK.  You might need to take this up with GTAC as it might require looking more closely at your part files.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: Part family component and assy constraints

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Was the "maintain relationships" option turned on in the replace component settings?

Re: Part family component and assy constraints

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor
I wonder if you need assign a name attribute to the face and then constrain to the named face...

Re: Part family component and assy constraints

Gears Phenom Gears Phenom
Gears Phenom

I mentioned the "maintain relationships" to the user, and they will check.  

 

I'm hoping to create a test assembly this afternoon, using the same part family.

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: Part family component and assy constraints

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor
I just tested NX10 with Tc10 and it worked with a basic assembly without needing to name the faces. With maintain relationships unchecked the constraints were removed. With maintain relationships checked the contraints updated with the replacement component.

Re: Part family component and assy constraints

Gears Phenom Gears Phenom
Gears Phenom

In my test, everything worked as expected.

 

For now, I'm going to chalk this up to an operator error.

 

Thanks!

-Dave
NX 11 | Teamcenter 11 | Windows 10