Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Part history interogation

Master
Master

I was wondering if there was somewhere that I could see more than just who and when saves were but what changes were done to a file? Thanks

Shags72 Mfg. Eng.
Windows 10 Pro 64bit
NX 11.0.2.7 MP2 Teamcenter 11
Dell M7720 i7-6820HQ 16GB RAM,
NVIDIA Quadro P3000
3 REPLIES 3

Re: Part history interogation

Siemens Phenom Siemens Phenom
Siemens Phenom

You can check by
Menu > Information > Part > Part History and Modifications.

 

From part navigator columns Created, Modified, Created By, Modified By can be useful to certain level but 'Part Modifications' have several options to know modifications using old version(s) of part alongwith criteria and object types.

 

Re: Part history interogation

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @shags72 ,

 

There are some tools that would be helpful to you to track changes:

 

  1. Display part modifications information: This command can be used to see the modifications in the part. It will generate Part Modifications Report based on comparison criteria.
  2. Model Compare: This will help you to compare geometries within part files or between 2 part files. Of course you'll need old geometry or original part to compare with.
  3. Track Drawing Changes: This will help you to track changes in drawing. You'll need to save snapshot data first and then you can compare later on whenever you want to do.

Also take a look at this post: HOW TO COMPARE TWO PARTS/MODELS

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

Re: Part history interogation

Master
Master

Thank you both! I will take a look at these ideas.

Shags72 Mfg. Eng.
Windows 10 Pro 64bit
NX 11.0.2.7 MP2 Teamcenter 11
Dell M7720 i7-6820HQ 16GB RAM,
NVIDIA Quadro P3000