05-18-2018 01:11 AM
05-18-2018 05:14 AM
what is the callout attribute in the properties of that part?
05-18-2018 05:30 AM
The […] in the Item field indicates that more than 1 components ‘Name’
share the exact same value, but the ‘CALLOUT’ attribute are set to
different values.
05-18-2018 01:55 PM
Use the "Key Field" checkbox in the column's settings to identify distinct values:
Regards, Ben
05-21-2018 04:14 AM
Ok "Key Field"-check box made them appear.
11-23-2018 06:44 AM
This NX \ TC bug appears still now and then sometimes...
Like 300pcs of same bolts and somehow like 2pcs of the same bolts are seperate and triple dotted.
Like this(Example): NX11+TC11
Pos. Qty Name_____
23 300 M8x20 Bolt
(...) 2 M8x20 Bolt
Any reason why this happens ?
11-23-2018 07:03 AM
Probably the CALLOUT Attribute requires editing to match, I think it comes down to when they were added and the Assembly was saved.