Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Part list fine tuning. Combining 2 column ?

Genius
Genius

Hi

Part list was so large it got separated (photo).

  • How to combine both in a 1 column ? Now it is in 2 columns.

cONNECT.png

2 REPLIES 2

Re: Part list fine tuning. Combining 2 column ?

Valued Contributor
Valued Contributor

In NX8.5.3, RC on Parts list. Go to Style. Go to Sections tab. Change Maximum Height as req'd. Hopefully NX9 has similar screens to go to.

Re: Part list fine tuning. Combining 2 column ?

Experimenter
Experimenter

Hi 12131444,

 

The issue is with the Max. table height preset - this limits how tall the table can be (which is where the table split will occur).

 

Hope this example helps;

 

 


1.jpgTable settings2.jpgSection Max Height3.jpgMax height adjusted