Cancel
Showing results for 
Search instead for 
Did you mean: 

Part list in drafting doesn't work (NX10)

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

When I try to create part list in drafting no all parts appears in table.

There should be over 80 parts but in part list (red boundry) appears only 4. Pls check the attachment. 

 

 

 

part list_problem.jpg

 

9 REPLIES 9

Re: Part list in drafting doesn't work (NX10)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The parts list is generated from the components in the assembly. Take the same screenshot, but with the assembly navigator open.

 

Also, check the "assembly levels" of the parts list. This option can be changed to show different levels of the assembly. If the 4 items that show up in the list are themselves sub-assemblies, then the "assembly levels" option is probably not set to what you want.

 

Another thing to look out for is "drafting components"; these are views added from other part files. They add a special icon to the assembly navigator, but they do not appear in the parts list.

Re: Part list in drafting doesn't work (NX10)

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

thanks a lot for respond. Here you have the screenshot with assmembly navigator openpart list_problem.jpg

Re: Part list in drafting doesn't work (NX10)

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

and are you able to explain me how to set the assembly levels in correct way? Because you are right, now in part list the subassemblies only appears that why there is only 4 position in the table. Thanks a lot!

Re: Part list in drafting doesn't work (NX10)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Right click on the parts list and choose "edit levels"; a dialog will open with a few toggle options. Have a look at the help file for what each one does:

 

https://docs.plm.automation.siemens.com/tdoc/nx/10/nx_help/#uid:index_drafting:id702253:id702353:id7...

Highlighted

Re: Part list in drafting doesn't work (NX10)

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

and I have the last question in this topic. When I try to create part list in the sheet which is show below some error apear. Do you know maybe how I can solvce it?part_list_problem_2.jpg

Re: Part list in drafting doesn't work (NX10)

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

It's not an error, but a warning.  You're attempting to add multiple parts lists to your drawing file.

 

By default, UGII_UPDATE_ALL_ID_SYMBOLS_WITH_PLIST is set to a value of 1.  This value prevents you from inserting multiple parts lists in a single part file and allows ID symbols (balloons) to synchronize with the item numbers in the parts list.

You can set this variable's value to 0, which allows multiple parts lists to be inserted, however, your balloons will not update with any of the parts lists.

The variable is set in the ugii_env_ug.dat file found here: %UGII_BASE_DIR%\UGII, which is typically here: C:\Program Files\Siemens\NX XX.XX\UGII\

It is advised that changes to the OOTB variables are defined in the accompanying environment file: ugii_env.dat (found in the same location as ugii_env_ug.dat), which makes it easier to monitor which variables have been edited.

 

Regards, Ben

Re: Part list in drafting doesn't work (NX10)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

"It's not an error, but a warning."

@BenBroad

 

I agree that this is more of a warning situation rather than an error; but to make that clear, Siemens should use the warning icon (exclamation point on yellow background) rather than the big red X, and get rid of the word "error" in the message box title bar.

Re: Part list in drafting doesn't work (NX10)

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor
@cowski1 - agreed. I'll submit an internal PR suggesting that this is corrected.

Re: Part list in drafting doesn't work (NX10)

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

thanks a lot. I have one more question to this drawing. Are you able to answer me why I can not make autoballon on isometric view and detaile view at the same time?autobaalloon1.jpgUntitled.jpg