Cancel
Showing results for 
Search instead for 
Did you mean: 

Part name in balloon

Phenom
Phenom

Hi,

we want to use the part name in the ballooning instead of callout, but for part name less more long the standard, the text goes outside the underline.

Exist a setting to position the text on the left and the underline grow related to the text length ?

2018-05-04 15_49_22-NX 11.0.2.7-NEXION INDUSTRIAL GROUP - Drafting - [2019251B_TAV1.prt].png

Thank you...

Using NX1859
RuleDesigner PDM

16 REPLIES 16

Re: Part name in balloon

Valued Contributor
Valued Contributor

Would something like this work?

 

text in balloon.JPG

 

 

 

 

 

Re: Part name in balloon

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Would it be something with text origin?

Try setting the text origin to "lower left"? 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Part name in balloon

Phenom
Phenom

Hi @Mark-J,

yes, can you tell me the setting ?

Thank you...

Using NX1859
RuleDesigner PDM

Re: Part name in balloon

Phenom
Phenom

Hi @Ken_A,

can you shot an image with settings, because I can't find.

Thank you...

Using NX1859
RuleDesigner PDM

Re: Part name in balloon

Valued Contributor
Valued Contributor

Here are the settings. I changed the settings size to 1.0 to get the text to fit.

 

text in balloon NX window.JPG

Re: Part name in balloon

Phenom
Phenom

baloon setting.pngHi @Mark-J,

I've verified the setting and are the same, but the result doesn't change. What NX version have you ?

 

Thank you...

Using NX1859
RuleDesigner PDM

Re: Part name in balloon

Gears Phenom Gears Phenom
Gears Phenom

@cubalibre00,

Either right click on the Balloon and select Settings or double click it to bring up the dialog above and click on the Settings button. Both methods will get you where you need to go, which is the Settings dialog for the Balloon. Under the Settings dialog, change the balloon size to a larger value such that the text fits.

Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.5.1

Re: Part name in balloon

Phenom
Phenom

Hi @TimF,

I've found the setting like before, but entering the '1' as the image, I thoight that the value '1', fit automatically.

It's not so, for each text I need to find the exact value.

Doesn't exist a setting for the auto-fit ?

Thank you...

Using NX1859
RuleDesigner PDM

Re: Part name in balloon

Gears Phenom Gears Phenom
Gears Phenom

@cubalibre00,

 

No, I do not believe there is an Auto Fit.  If your part numbers all have the same number of characters, you can find the correct setting then select all the others and apply to all using inherit.  The Auto Fit would be a half-way decent ER, I would think.

 

If the part numbers are of differing character lengths and you're not going to change the text settings, I would suggest finding the one with the most characters and using that value for all of the balloons.

Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.5.1