Cancel
Showing results for 
Search instead for 
Did you mean: 

Parts list text change color after level edit

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Attached the parts list template I would like to use in NX10. (Sorry I would like to attach it but I'm unable to attach any of this: .prt, .zip, .7z)
Any way I think it is ok (but perfectable).

When insert the template the text are red colored
If I edit levels and the rows change, the text color became of the same color of the cells border.

Is this as designed? Why?

 

TY

 

Finally able to post attachment (adding and _ at the end of extension). What type of file this forum support for attachments?

Fabio
I use NX18xx with Gerrit Koelewijn configuration utilities. Thanks to Rob Cohon.
1 REPLY 1
Highlighted

Re: Parts list text change color after level edit

Valued Contributor
Valued Contributor
I had similar problem. I do not have v10 so I’m going to take a stab but I would like more tips also. When you create a *template*, set all of the cells of the Tabular Note to the formatting you want any *added cells* to be. This should be a default for the Tabular Note. If any rows or columns are to be different, make sure you select by Rows or Columns. Then, if you want special title format rows or cells, change them last.
Please correct this if it is wrong.
Cord