Cancel
Showing results for 
Search instead for 
Did you mean: 

Pasting an image in drafting?

Legend
Legend

Is there a way to just copy and paste an image into a drawing sheet?

 

I use one of the journals on the NX journaling site to grab an image to paste in office apps.

Is there a way to take this image in the clipboard and paste in onto a drawing sheet without having to save as a an image 1st then inserting it into the Drawing?

 

 

Rob Newcomb, CAD/CNC/Simulation manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r7 /WorkNC 2018 r2
Testing:NX EAP
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro
1 REPLY

Re: Pasting an image in drafting?

Siemens Phenom Siemens Phenom
Siemens Phenom

Pasting a JPG or other image file into a drawing is not supported. However, a slightly easier option than using the insert command is to drag and drop the image file from an explorer window into the drawing sheet.

 

Abe

Regards,
Abe