Cancel
Showing results for 
Search instead for 
Did you mean: 

Pc spec for NX 3D modelling /rendering

Pioneer
Pioneer

Hi,

 

My PC spec :

Win 7 professional  SP1 -64bit
Intel Xeon CPU E3-1220 v5 @ 3Ghz
16GB RAM
Nvidia Quadro P1000

 

Will above spec able to run 3d modelling + photorealistic rendering with NX 7.5 onwards until NX12 + Iray rendering ?

 

thanks.

 

Jerman

5 REPLIES 5

Re: Pc spec for NX 3D modelling /rendering

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

NX12 and Windows 7 are only partially supported. The rest looks good to me.

Re: Pc spec for NX 3D modelling /rendering

Pioneer
Pioneer

Do CPU hyperthreading improved nx rendering speed ?

Re: Pc spec for NX 3D modelling /rendering

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Rendering is fastest when dont through Nvidia Iris compatible Graphics card.

CPU Rendering is used as an alternative when no compatible graphics card is available. Hyperthreading should have no effect on rendering speed.

Re: Pc spec for NX 3D modelling /rendering

Gears Phenom Gears Phenom
Gears Phenom
Hi @jerman,

Get as much as you can afford - if possible the more or faster, the better.
Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.6

Re: Pc spec for NX 3D modelling /rendering

Experimenter
Experimenter

3D rendering softwares are intensively using the graphic card and CPU features. The software has been built to use these features. If your computer doesn't have these features, you cannot use them properly or use the software at all... Thus, recommended hardware on which the software has been proved to work.
It doesn't mean you must have those hardware, but you might experience glitches.


Cheers,

Adrian Gates

System Admin at CloudDesktopOnline