Cancel
Showing results for 
Search instead for 
Did you mean: 

Pipe thickness measure in NX ?

Genius
Genius

Hello

What to click to get the pipe's thickness properly ?

  • Blue arrow marks the sketched measure-style that I want to create.

measure56446.jpg

2 REPLIES

Re: Pipe thickness measure in NX ?

Phenom
Phenom

There is the appropriate command.

 

Re: Pipe thickness measure in NX ?

Siemens Phenom Siemens Phenom
Siemens Phenom
Hello @12131444,

I think you have used the rapid dimension. This is what it is, it creates rapidly a dimension and the one that you want in 80-90% of the time.
For the other 10-20% of the dimensions, you need to select the specialised dimensions, like explained by @Cesare.

Kind regards,
Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software