Cancel
Showing results for 
Search instead for 
Did you mean: 

Plotting in NX10

Pioneer
Pioneer

I am setting up NX10.0 using the NX100Custom method that I got from here.

I have been into the Printer Administration to setup the plotter but when I go to plot I don't get the plotter in the printer field, all I get are image formats.

Any Ideas.

1 REPLY

Re: Plotting in NX10

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Did you set the variable UGII_SDI_SERVER_CFG_DIR to point to the location of the plot configuration you created through printer admin?

Also the following variables should be set to point to a temp folder (e.g c:\temp):

UGII_SDI_BPS_JOBS_DIR & UGII_SDI_OVERRIDE_HOME

Anthony Galante, Senior Support Engineer
PhoenxPLM
24 versions of NX installed: NX4 to NX12, plus TC11.2