Cancel
Showing results for 
Search instead for 
Did you mean: 

Point at intersection of surface and datum axis?

Honored Contributor
Honored Contributor

Any way to do this, without creating a bunch of other datum planes, and intersection curves?   NX9

-Dave
NX 11 | Teamcenter 11 | Windows 10
6 REPLIES 6

Re: Point at intersection of surface and datum axis?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Dave,

 

use the Point Set command and change the Type to "Intersection Points". The rest is pretty discoverable.

 

Regards,

Johannes

Re: Point at intersection of surface and datum axis?

Honored Contributor
Honored Contributor
Thanks Johannes! I would not have thought to use "point set".
-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: Point at intersection of surface and datum axis?

Experimenter
Experimenter

Does anyone know of a grip proram to export XYZ location and datum axis vetor direction

Re: Point at intersection of surface and datum axis?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@WSC_Engineer,

This would be a good topic for a new thread in the programming forum. That said, I don't know that you will get many answers for GRIP, but it would be a fairly simple journal to program.

 

Here is a thread with a similar request:

https://community.plm.automation.siemens.com/t5/NX-Design-Forum/Points-and-vectors/m-p/340947/highli...

Re: Point at intersection of surface and datum axis?

Creator
Creator

This solution is not working for me. The 'Curve' selection field within the Point Feature definiton dialog, as well as the Point Set Feature definition dialog, is not allowing the selection of a 'Selection Axis' Feature nor 'Selection Axis' sub-feature. I am using NX 8.5.3.3.
Is this one of those features that has been improved in later versions?

Re: Point at intersection of surface and datum axis?

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Correct.  This was not possible using the Point Set command in NX 8.5.  Here's a side by side of NX 8.5 and NX 11 Point Set dialogs:

 

 Screenshot - 2_13_2018 , 3_11_54 PM.png

 

Regards, Ben