Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Point size

Gears Phenom Gears Phenom
Gears Phenom

NX 9

 

I have a user that would like to increase the size of a "point" in the modeling application.  Is there a setting for this?  I haven't found it yet, but may be searching for the wrong thing.

 

Thanks,

-Dave

-Dave
NX 11 | Teamcenter 11 | Windows 10
2 REPLIES

Re: Point size

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi Dave,

 

Go to the Visualization Preferences, select the View/Screen tab and select "Calibrate" located within Session Settings.  With "Lock Resize Sliders" toggled on, drag one of the sliders to increase the resolution and Apply the change (make sure you have a point on the screen when you do this - it will also increase the size of other objects - have a Datum CSYS displayed as well as the point for comparison).  It's not what this command was intended for, but it works for users that request this capability.

 

Regards, Ben

Re: Point size

Gears Phenom Gears Phenom
Gears Phenom

Thanks Ben.

-Dave
NX 11 | Teamcenter 11 | Windows 10