Cancel
Showing results for 
Search instead for 
Did you mean: 

Possible to create twisted , revolved body in sheet metal

Pioneer
Pioneer

Hi,

 

It is possible to create twisted  and revolved sheet body in nx cad8.5? 

3 REPLIES 3

Re: Possible to create twisted , revolved body in sheet metal

Siemens Phenom Siemens Phenom
Siemens Phenom

It greatly depends on the shape. The basic NX sheet metal application is meant for straight break sheet metal parts. Some features, such as contour flange enable you to create rounded shapes. However, complex sheet metal shapes can be created either as modeling features with a specific material thickness or in some cases using the  Aerospace sheet metal application.

Regards,
Abe

Re: Possible to create twisted , revolved body in sheet metal

Legend
Legend

Generally, you may modeling complex boby from Modeling App.
And then, you can convert the body to Sheet metal body with 'Convert to Sheetmetal' command.
If the body has same thickness, the result will successful and you can add Sheet metal Features, additionally.

 

Please refer this document

Recommended workflow to create enclosures with odd shapes or angles

 Sunkap Ahn, Senior Support Engineer


logo

Re: Possible to create twisted , revolved body in sheet metal

Pioneer
Pioneer

Thanks

 

Pls provide some videos for this.